TE - White Papers

Lighting System Interconnection Levels

Issue link: https://te.mouser.com/i/1410851

Contents of this Issue

Navigation

Page 16 of 19

connector on the driver board, or as simple as a wire nut connecting the wire from a lamp to a wire from the driver/ballast. Of course, since most incandescents do not require an intermediate power source, most incandescent lighting fixtures do not have a Level L4. L4 L4 Fig.21 LED desk lamp Fig. 22 LED recessed fixture L5 L5 Fig. 23 AC power connection Fig. 24 Fluorescent troffer connections Continuing away from the lamp, we come to Level L5 which is the primary power connection to the fixture. This is a separable connector and is typified by a standard plug and receptacle configuration. In North America, this is the NEMA compliant two or three prong plug. In Europe and other locations, this is the DIN two pin plug. Since industry standard AC plugs are used, in most instances, this is a 120VAC/220VAC/277VAC/347VAC power source for most lighting applications. In some regions of the world, electrical codes allow recessed lighting fixtures to be pluggable using a Tyco Electronics NECTOR connector or equivalent as the primary power connection. Also worth mentioning at this point is that there are a number of efforts taking place around the globe that promote low voltage DC as a primary power source for lighting. Immediately below is 15

Articles in this issue

view archives of TE - White Papers - Lighting System Interconnection Levels