TE - Solutions Guide

Lighting Solutions

Issue link: https://te.mouser.com/i/1410845

Contents of this Issue

Navigation

Page 27 of 50

The variability of COB thickness poses yet another design challenge for a socket product. COB substrates are available in a variety of materials and thicknesses that need to be accommodated. The thinner and more brittle ceramic packages can easily crack under pressure when used with flexible thermal interface pads and therefore consequentially commonly use greases as TIMs. On the other hand, the more durable aluminum substrates commonly use grease or flexible TIM materials. Any holder being considered by a manufacturer needs to be evaluated relative to how it accommodates these varying stack heights posed by COB applications. One method is commercially available that utilizes a combination of optional thermal springs and housing ledges to accommodate both types of COBs. An example using aluminum substrate COB is shown in Fig. 13 below. The same system when used with the thinner ceramic substrates is shown in Fig 14 with clearance to avoid exerting screw pressure on the ceramic substrate . Fig. 13 Fig. 14 Copyright 2018 TE Connectivity Ltd. Family of Companies TE Connectivity, TE connectivity (logo) and TE (logo) are trademarks. Other logos, product and/or company names might be trademarks of their respective owners.

Articles in this issue

view archives of TE - Solutions Guide - Lighting Solutions