TE - White Papers

Automotive Connector Strategies and Solutions for Space Saving

Issue link: https://te.mouser.com/i/1349209

Contents of this Issue

Navigation

Page 10 of 12

Automotive Connector Strategies and Solutions for Space Saving Page 11 TE AUTOMOTIVE /// White Paper | Automotive Connector Strategies and Solutions for Space Savings LITESURF plating technology is the result of more than five years of research and development to inves- tigate a tin-free plating that relieves the risk of whisker-induced failures and is suited to the high-stress conditions of press-fit pin connections. LITESURF plating was developed to meet manufacturers' needs for progressive miniaturization, reduced pin pitch, and a smaller connector footprint on PCBs. As TE developed the LITESURF plating technology, more than 12 different deposit compositions were researched, investigating whisker formation as well as other behavioral characteristics impacting produc- tion processes such as melting temperatures. TE experts created a detailed matrix of all options. The TE study concluded that the optimal deposit for plating was an electroplated Bismuth-based coating. Using Bismuth has additional benefits, allowing manufacturers to use an application process that follows the typical galvanic plating line procedure that is comparable to a standard tin bath. Bismuth-based LITE- SURF plating can be implemented within existing plating lines without any additional process changes. Extensive LITESURF plating tests were performed on more than 5,600 multi-spring and action pins and on three different types of PCB technologies. Tests demonstrated that LITESURF plating can reduce the risk of whisker incidence by a factor of over 1,600, based on the number and size of particles detected combined with Bismuth's lower conductivity, which is 90 percent lower than tin's conductivity. Figure 12. LITESURF anti-whisker plating composition

Articles in this issue

view archives of TE - White Papers - Automotive Connector Strategies and Solutions for Space Saving