TE - eBooks

Connected LED Lighting Solutions

Issue link: https://te.mouser.com/i/1475713

Contents of this Issue

Navigation

Page 4 of 35

mouser.com/te 5 FIGURE 1: The image shows the driver is permanently powered in the Zhaga architecture. (Source: TE Connectivity) The D4i digital communication protocol was created through a liaison between Zhaga and the DALI Alliance. This protocol has baked in arbitration, creating a hierarchy between two control devices on the same bus. As shown in the Zhaga architecture image, the driver is now permanently powered (Figure 1). Typically, an AUX 24VDC PSU is built into the driver, although a separate PSU is allowed. This means that a 24V rail is always available, creating opportunities for communication and sensor-node designs that can be used at any time of day. Wiring becomes simplified with the two control devices and the driver connected to the same communication bus. This edition also defined the power budget that the driver is required to deliver from both the AUX power supply and the powered DALI bus power supply—as well as the power that different types of control devices are allowed to pull from the system. This is all controlled through a certification program. Drivers are certified D4i by the DALI Alliance, while luminaires and control devices are certified Zhaga- D4i by the Zhaga Consortia.

Articles in this issue

Links on this page

view archives of TE - eBooks - Connected LED Lighting Solutions