TE - eBooks

Connected LED Lighting Solutions

Issue link: https://te.mouser.com/i/1475713

Contents of this Issue

Navigation

Page 24 of 35

mouser.com/te 25 Harvesting plants produced inside greenhouses are set to greatly increase over the next several decades. This is in response to advancements in LED technology. Annual growth rate projections for urban farming exceed twenty-five percent (25%). Europe is the continental leader in this field. It is expected that the Asia Pacific region, which is undergoing a faster rate of urban development, will ultimately become the global leader over the next generation. Growing plants through urban farming eliminate the need for long-haul transportation, placing it closer—urban farm to table. As issues related to lighting, power, and runoff are successfully dealt with, the adoption of urban farming methods will quicken. FIGURE 1: Flowers growing with LED light on an indoor farm. (Source: Adobe Stock) Color LEDs Enable Growing Opportunities Urban farming typically employs artificial light as opposed to natural sunlight. LEDs are rapidly becoming the light source of choice (Figure 1). For indoor horticultural applications, LEDs can customize the light spectra to meet the growth and nutritional needs of the plant of interest— something that legacy horticulture light sources don't do. LEDs also have superior lifetimes, greater energy efficiency than fluorescent tubes used in vertical farms and plant factories, require little to no maintenance and emit less heat. With the development of a wide variety of color LEDs, the urban farmer is no longer dependent on natural light sources. Electronically controlled, LEDs can

Articles in this issue

Links on this page

view archives of TE - eBooks - Connected LED Lighting Solutions