TE - White Papers

The Future of Connected & Electrified Powertrains in Vehicles

Issue link: https://te.mouser.com/i/1450917

Contents of this Issue

Navigation

Page 4 of 6

5 POWERTRAIN REVOLUTION According to the provisions of the Economic Commission for Europe regulation "ECE R-100, Battery-Powered Electric Vehicles," battery-powered vehicles must, in general, be equipped with protection devices such as fuses, circuit breakers or main contactors in case the traction battery becomes overheated by overcurrent. At the same time, the short circuit capability could be improved versus previous designs to a level of 6kA. When currents of that magnitude pass a pair of closed switching contacts, the associated Lorentz force generates a levitation force that tends to push the contacts open. This force increases with the square of the current. At 1kA, the force reaches already about 1N. If the current is high enough, the contact spring force is compensated and the contacts will separate, immediately forming a severe arc. As a consequence, the contacts could either weld when reclosing, or the contactor could rupture due to the excess pressure developing in the contact chamber. With the increased levitation limit of 6kA and the unsealed design of the contact chamber, the risk for such failure modes is significantly reduced with the EVC 250 contactor. New generation EVCs With the EVC 250 high voltage contactor, TE launched a new generation of high voltage automotive contactors that work without a sealed contact chamber and without pressurized inert gas. This not only eliminates a complex and expensive manufacturing process, but also improves the functional reliability of the device. A potential gas loss is not an issue anymore. In addition, it eliminates the need for any preventive actions, such as a regular replacement of the contactor during vehicle maintenance. More recently, TE launched the EVC 175 contactor which is the latest new product in the growing contactor portfolio. The EVC 250-800 contactor provides a solution for hybrid and electric vehicles with higher system voltages up to 900V. The latter is based on the well-known EVC 250 contactor, but features increased creepage and clearance distances that fulfill the isolation requirements of IEC 60664 for up to 1,000VDC. With this lineup of innovative high voltage contactors, TE provides advanced switching solutions to the automotive industry, supporting and enabling a continued and successful growth in the market for electric powertrains in passenger cars as well as commercial vehicles. Improved charging technology critical to growth of electric powertrains Charger cable is one of the key components supporting the e-mobility trend. It is seen as a major element for the satisfaction of the end customer, considering that the complete functionality of the car is depending on it. TE delivers to several OEMs both Mode 2 and Mode 3 charger cables according to the IEC 62196 standards for different regions and countries. TE connectors are designed to survive the harshest environment such as being able to mate more than 10,000 times. To support this robust design, TE connectors are ultrasound welded for excellent sealing performance as well as breakage resistance.

Articles in this issue

Links on this page

view archives of TE - White Papers - The Future of Connected & Electrified Powertrains in Vehicles