TE - Articles

Key Drivers of Growth Acceleration in the Commercial Drone Market

Issue link: https://te.mouser.com/i/1416839

Contents of this Issue

Navigation

Page 8 of 9

KEY DRIVERS OF GROWTH ACCELERATION IN THE COMMERCIAL DRONE MARKET / TREND PAPER Key Drivers of Growth Acceleration in the Commercial Drone Market PAGE 9 • Connectors – Designed to reduce application size while managing power usage and enabling increased performance in the harshest conditions. We offer IP67 rated sealing options and ergonomics-friendly connectors that are glow wire tested and come with optional TPAs and connector position assurance (CPA) for extra protection, with operating temperatures up to 110°C. • Sensors – Whether you're designing drones that need to measure pressure, temperature, position, vibration, or humidity, our engineers can help bring your ideas to reality using intelligent, efficient and high-performing TE sensors proven in harsh environments. • Terminals – TE's terminals are ergonomically friendly (low insertion force) and designed for high retention with optional terminal position assurance to stay mated under extreme vibration or shock such as drone collisions. • Antennas – With the ability to maintain high-quality transmissions in wireless devices, our broad range of standard and custom antennas can transmit reliably using 5G, LTE, Cat-M, NB-IoT, GNSS, Wi-Fi, Bluetooth, V2X, ISM and LPWAN bands and more. TE has antenna design and manufacturing facilities worldwide, with testing capabilities in near- and far-field patterns, scattering parameters, specific absorption rate (SAR), vibration, humidity, temperature shock, salt fog, throughput and acoustics. The choice of antenna can be critical to a device's reliability and function, and since antennas are commonly embedded as part of the device they must be considered from the start of the concept and design process. • Board-level shielding – With the growing demand for thinner devices with multiple antennas, higher data rates, and increased operating frequencies, modern mobile devices require better solutions for reducing or limiting the effect of electromagnetic interference (EMI). Board-level shields from TE are stamped one-piece and two-piece metal cages that help isolate board-level components, minimize crosstalk, and reduce EMI susceptibility, all without impacting system speed. • Heat shrink tubing – Designed to perform in the most demanding conditions, TE's heat shrink tubing portfolio comes in a wide range of single-wall, dual-wall and specialty options that seal, protect, and insulate the components that require the most protection. Depending on the drone you're designing, you may choose tubing that is resistant to high operating temperatures, chemicals, water and fluids, and/or flames, such as for drones used to monitor wildfires. How TE Connectivity Leads with Quality Engineering Solutions TE Connectivity (TE) has a broad portfolio of rugged and sealed connectors, terminals and tubing; a range of different sensors that have proven reliability and quality in uses across industries; and standard and customized antennas covering all current global cellular and LTE bands as well as active GPS/GNSS/Galileo/Beidou applications that need to send back data on position or timing. Wireless connectivity for outdoor applications presents a number of challenges with many potential sources of interference and signal blocking, such as inclement weather, tall trees and buildings, and more. Our product portfolios are designed with extensive engineering expertise to provide our customers with high-performing product solutions meeting a range of connectivity challenges and industry requirements. Many of our products are suitable for the harsh outdoor environments in which commercial drones operate. As a global industrial technology leader, TE is a design partner that innovates alongside you, sharing our expertise gained from extensive cross-industry experience. We understand how connectors, sensors and other components work together and use this knowledge to optimize performance and create more connected, more sophisticated commercial drone designs to drive safety and reliability for current and potential applications. Finding ways to solve customer design challenges while maintaining or increasing reliability and performance in harsh environments is just one of the ways TE lives up to its purpose of creating a safer, sustainable, productive and connected future. TE Connectivity has high-performing engineering solutions with proven reliability for drone applications.

Articles in this issue

Links on this page

view archives of TE - Articles - Key Drivers of Growth Acceleration in the Commercial Drone Market