TE - eBooks

TE Proven in the Harshest Environments

Issue link: https://te.mouser.com/i/1385324

Contents of this Issue

Navigation

Page 23 of 37

24 Proven in the Harshest Environments The DT family relies on an extensive series of modifications used when part configuration changes are made to a basic connector version. They include flange adapters, styles, types, keys, colors, caps, and integrated electronic components as resistors and diodes. Approximately 300 choices are available. Many features can be aggregated into a combination modification, such as the popular CE10 modification, including the CO15 E-seal grommet plus EO4 black color housing in a PO12 enhanced seal-retention attribute. The splitter product is the PO7 CAN splitter, a three-way, three-position part shown above in Figure 6, and DT detector parts with a status indicating on and off LEDs for both 12- and 24- volt applications used on several solenoid valve applications in vehicles. The DT family requires wedge lock-in seals for both plugs and receptacles and the wedge locks used to retain the terminals in place securely. They also ensure contact alignment, secondary retention, and are sold separately. DEUTSCH launched its DT snap-cap product line in 2019 and continues to build upon this global platform with product enhancements and variations. For example, new plating options will offer price savings over gold while maintaining performance. Next-generation designs will also continue to improve ergonomics and handling. TE Connectivity provides customization for its customers. Often this customization has broad market use, and in those instances, that can lead to further parts for the complete customer base. That's why more than 8,300 products are in the TE Connectivity portfolio—proof that TE Connectivity has listened to customers for decades and is successful in bringing innovative solutions to market. The DT 06-2 S series plugs shown on the left contain PO12 enhanced seal retention, along with an associated wedgelock, the W2 SPO12. DT series connectors are available with a reduced diameter rear grommet, referred to as an E-seal for small wire insulation found typically on ISO-grade wires and available as a modification of most DT family of products. These seals are readily identified with the E and a circle marking on the grommet or laser welded on the seal cap when outfitted with a cap. FIGURE 6: DT Family Modifications. (Source: TE Connectivity) FIGURE 7: DT Family Wedgelocks and Seals. (Source: TE Connectivity)

Articles in this issue

view archives of TE - eBooks - TE Proven in the Harshest Environments