TE - White Papers

Automotive Connector Strategies and Solutions for Space Saving

Issue link: https://te.mouser.com/i/1349209

Contents of this Issue

Navigation

Page 6 of 12

Automotive Connector Strategies and Solutions for Space Saving Page 7 TE AUTOMOTIVE /// White Paper | Automotive Connector Strategies and Solutions for Space Savings can be locked at up to 20 positions without the need for reinforcement ribs. In addition, the plastic locking and latching profiles have compact geometries. For example, the overlap between the connector and header fronts has a wedge shape that ensure a smooth guiding-in of the two halves during connector mating. When fully mated, the overlap results in a strong, positive connection formed by two wedge shapes securing each other. 8 | HOW NanoMQS TERMINALS DELIVER UP TO 50% SPACE REDUCTION NanoMQS series terminals are designed for a nominal pitch, corresponding to the distance between the pins connecting with the PCB of 1.8 millimeters. Therefore, the same number of positions on a NanoMQS header requires only approximately half the space on a PCB compared to an MQS header needs (Figure 6). As depicted in the figure, the header footprint of the MQS plat- form is reduced from 840 mm 2 to 411 mm 2 with NanoMQS system. Clearly, high-position intercon- nections will be much in demand with next-generation car architec- tures with significant packaging density. In an engine ECU Nano- MQS terminals could save 60 per- cent of the ECU's spatial footprint. Current NanoMQS terminal ver- sions can accommodate up to 320 positions. This makes the NanoMQS platform ideally suited for hybrid connectors, as every contact of the MQS family can be integrated into a grid as a multi- ple of the next size up (Figure 7). This capability is enabled by the fact that the secondary locking device is on the same level on all housings. Figure 6: NanoMQS header (left) compared to a MQS header. Figure 7: NanoMQS connector variants with a common interface

Articles in this issue

view archives of TE - White Papers - Automotive Connector Strategies and Solutions for Space Saving