TE - White Papers

The Car in the Age of Connectivity

Issue link: https://te.mouser.com/i/1349134

Contents of this Issue

Navigation

Page 7 of 9

DRIVING TOWARD AN EMISSIONLESS FUTURE IN TRANSPORTATION THE CAR IN THE AGE OF CONNECTIVITY — H D B a s e T — HDBaseT is an emerging technology, providing up to 6Gbps (6 billion gigabit/second) full duplex data transmission, through a 15m link segment, with up to 4 inline connectors at near zero latency. It includes various protocols, such as audio and video, Ethernet, power, and consumer applications including USB and HDMI. TE has an active part in the HDBaseT Alliance, where automotive stakeholders collaborate in various technical committees to define appropriate automotive requirements and specifications. Native Networking Capabilities demonstrates the usability of unshielded twisted pair cabling, which can be compared to 100 and 1000 BASET1 applications. Addressing multiple challenges, HDBaseT with its unprecedented bandwidth and suitability for existing UTP cabling systems like TE's MATEnet is a key enabler for future in-vehicle connectivity. DATA AND THE DECENTRALIZED CLOUD Making full use of the capabilities of the 5G-enabled cloud will require faster, more robust in-vehicle data networks as well as a new generation of 5G native antennas, receivers, and connectors. But, in a future with billions of mobile devices and trillions of Internet of Things (IOT) moving massive amounts of data, it will also mean evolving the architecture of the cloud away from a centralized model to one where computing applications, data, and services are pushed to the periphery (the "edge") of a network. 10 With Edge Computing, speed is a key parameter. For instance, with Mobile Edge Computing (MEC), the current goals are: data rates up to 6 Gbps, less than 1 ms latency, mobility at 500 km/hour, and terminal localization within 1 meter. What this means in practical terms is more continuity of service with high reliability. 11 In situations where computing and response need to be instantaneous (i.e., with real-time traffic reports), these decentralized nodes would handle the data loads. Computations for things like autonomous driving would also be handled at this level. The centralized cloud core would still handle applications. Applications that require robust computing power, data aggregation, and data storage. TE's long history of partnering with leading enterprise and hyperscale customers—combined with our experience in data and devices—offer OEMs practical intelligence that will help them evolve vehicle technology toward making possible new opportunities in networked intelligence. THE TE ADVANTAGE: CROSS-DISCIPLINE INTELLIGENCE No matter which technology path OEMs choose to innovate for the connected car, TE partners with these customers early in the design process to accelerate innovation. By applying our expertise in automotive standards and knowledge we' ve gained from decades of working with customers, we can quickly meet evolving challenges and requirements in designing for the automotive industry. Today, there are two developments driving the automotive industry towards compact, robust high-speed communication solutions: ever-increasing data rates and the demand for miniaturization. A significant challenge around these developments is designing technology that maintains signal integrity. Although automotive manufacturers are now starting to talk about 10Gbps data rates, since the 1990s, we have manufactured 10Gbps products. We've shipped massive numbers of these high-speed components for almost 15 years. Combined with our understanding of automotive requirements, we are quickly adapting our solutions to meet the needs of automobile makers.

Articles in this issue

view archives of TE - White Papers - The Car in the Age of Connectivity